About Bourns | News | Blog | My Bourns | Partner Portals | Sales | Contact |  
Products Services Applications Design Kits Library Support RoHS Training
 
Site Search:       Advanced Search  
News
Press Releases
What's New
PR Images
Bourns Blog
Bourns Twitter
Tradeshows
Boilerplate
Press Contacts
 
 
 
 
 
 
2009 Press Release
Bourns Announces New Steering Diode Array Device Optimized for ESD, EFT and Surge Protection
Bourns Announces New Steering Diode Array Device  Optimized for ESD, EFT and Surge Protection
Download Hi Res Image (JPG 828KB)
Riverside, Calif., Jul 8, 2009 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of a new steering diode array that provides up to six lines of protection using the “rail to rail” clamping technique with low leakage current and low capacitance per line. Designated Bourns® model CDNBS08-SR112, the lead-free steering diode device was designed specifically for ESD, EFT and surge protection applications and is RoHS compliant.* Available in an NSOIC-8 package, the new device is designed to be mounted directly onto an FR4 printed circuit board. Bourns engineers optimized the design to protect a wide range of applications including Ethernet ports, portable electronics, wireless LANs and Universal Serial Bus (USB) interface-based systems.

Bourns’ steering diode array meets IEC 61000-4-2 (ESD), IEC 61000-4-4 (EFT) and IEC 61000-4-5 (surge) requirements for external ports and features very low capacitance of 5 pF to minimize electrical distortion. The devices also meet many worldwide, industry and government regulations regarding lead-free components and are designed for a variety of manufacturing environments, allowing the use of industry-standard “pick and place” equipment. The chip diode NSOIC-8 package offers simplified production with its flat configuration that minimizes rollaway.

"Bourns’ new steering diode array provides a good choice for ESD, EFT and surge protection for up to six communication data lines and also fits circuit board space constraints,” said Ian Doyle, ESD Product Line Manager for Bourns, Inc. “Bourns is pleased to offer the newest addition to the company’s steering diode array product line that meets industry demands for smaller electronic components with extremely low power consumption."


Electrical Characteristics (@ TA = 25 ºC Unless Otherwise Noted)
Parameter Value
Typical Forward Voltage @ 50 mA (V) 1.3
Repetitive Peak Reverse Voltage (V) 20
Maximum Peak Pulse Current @ 8/20 µS (A)
12
Maximum Leakage Current @ 18 V (nA)
20
Typical Junction Capacitance @ 0 V 1 MHz (pF) 5
ESD Protection per IEC 61000-4-2
Minimum Contact Discharge (kV)
Minimum Air Discharge (kV)

±8
±15
EFT Protection per IEC 61000-4-4 @ 5/50 ns (A)
40
Surge Protection per IEC 61000-4-5 @ 8/20 µs
L1 (Line – Ground) (A)
L2 (Line – Line) (A)

12
12


Pricing and Availability
Bourns’ new steering diode array device is available now. As a pricing reference, Bourns’ CDNBS08-SR112 is priced from $0.90-$0.95 in 10,000 piece quantities.

*RoHs Directive 2002/95/EC Jan 27 2003 including Annex.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

 


About Bourns

Bourns, Inc. is a leading manufacturer and supplier of automotive sensors, circuit protection solutions, magnetic products, microelectronic modules, precision potentiometers, panel controls and encoders and resistive products. Headquartered in Riverside, CA, Bourns serves a broad range of markets, including telecommunications, computer, industrial, instrumentation, automotive, consumer, non-critical life support medical, audio and various other market segments. Bourns products are manufactured according to ISO-9000 standards under Six Sigma quality programs. Additional company and product information is available at the company’s website at www.bourns.com.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Agency Contact:
Annette Keller
Keller Communication
(949) 640-4811
annettekeller@sbcglobal.net
  Company Contact:
Mikelyn Bridges
Bourns, Inc.
(951) 781-5397
mike.bridges@bourns.com