About Bourns | News | Blog | My Bourns | Partner Portals | Sales | Contact |  
Products Services Applications Design Kits Library Support RoHS Training
 
Site Search:       Advanced Search  
News
Press Releases
What's New
PR Images
Bourns Blog
Bourns Twitter
Tradeshows
Boilerplate
Press Contacts
 
 
 
 
 
 
2010 Press Release
Bourns Adds New Ultra-Low Capacitance Thyristor Surge Protectors to its TISP® Product Line
Bourns Adds New Ultra-Low Capacitance Thyristor Surge Protectors to its TISP® Product Line
Download Hi Res Image (JPG 828KB)
Riverside, Calif., Mar 23, 2010 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company has expanded its TISP® thyristor surge protector product line to include new ultra-low capacitance models that allow higher data rates to deliver improved VDSL2 performance while providing protection. The new Bourns® Models TISP4P015L1N, TISP4P020L1N, TISP4P025L1N and TISP4P035L1N address a range of popular chipset voltages. These new thyristor surge protectors are designed with a new lower capacitance process as an optimal circuit protection solution for ADSL, ADSL2, ADSL2+, VDSL and VDSL2 applications from overvoltages caused by lightning and AC line disturbances. Low capacitance reduces distortion and minimizes the effect of using circuit protection in sensitive equipment. The new devices can also be used for T1/E1 driver protection, in customer premise and central office locations and in any transformer-coupled interface, which leaves the building.

Bourns new TISP® devices are symmetrical, two-terminal thyristor-crowbar devices that can be deployed to protect from line to ground or between the differential driver conductor pair. When placed between the xDSL line driver IC and the transformer, the devices will clamp and switch into an ultra-low impedance state, safely diverting the energy and protecting sensitive equipment from dangerous overvoltage or line disturbance threats that can result in system failure.

"These new models offer significant competitive advantages for our customers,” said Beverley McKnight, product line manager for Bourns’ TISP® products. “These new protectors feature differential capacitance, typically less than 3 picofarad (pF), which makes them our lowest capacitance device. They enable reliable overvoltage protection that meets the faster data rates required by a broad range of VDSL2 applications. Bourns designed these new TISP® products to help our customers deliver high reliability and low cost solutions for their faster data rate products.”

Pricing and Availability
Bourns® Models TISP4P015L1N, TISP4P020L1N, TISP4P025L1N and TISP4P035L1N are available now. For complete specifications, go to Bourns’ website at  /ProductFamily.aspx?name=tisp. As a pricing reference, the new models are priced from $0.30 at 10,000 pieces.
About Bourns

Bourns, Inc. is a leading manufacturer and supplier of automotive sensors, circuit protection solutions, magnetic products, microelectronic modules, precision potentiometers, panel controls and encoders and resistive products. Headquartered in Riverside, CA, Bourns serves a broad range of markets, including telecommunications, computer, industrial, instrumentation, automotive, consumer, non-critical life support medical, audio and various other market segments. Bourns products are manufactured according to ISO-9000 standards under Six Sigma quality programs. Additional company and product information is available at the company’s website at www.bourns.com.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Agency Contact:
Annette Keller
Keller Communication
(949) 640-4811
annettekeller@sbcglobal.net
  Company Contact:
Mikelyn Bridges
Bourns, Inc.
(951) 781-5397
mike.bridges@bourns.com