About Bourns | News | Blog | My Bourns | Partner Portals | Sales | Contact |  
Products Services Applications Design Kits Library Support RoHS Training
 
Site Search:       Advanced Search  
News
Press Releases
What's New
PR Images
Bourns Blog
Bourns Twitter
Tradeshows
Boilerplate
Press Contacts
 
 
 
 
 
 
2010 Press Release
Bourns Integrates Two Polymer Positive Temperature Coefficient Resettable Fuses into a Single Package
Bourns Integrates Two Polymer Positive Temperature Coefficient Resettable Fuses into a Single Package
Download Hi Res Image (JPG 828KB)
Riverside, Calif., Mar 30, 2010

— Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company has integrated two polymer positive temperature coefficient (PPTC) resettable fuses into a single package. This new Multifuse® device contains twin 250V polymer PTC resettable fuses and decreases the circuit protection footprint by fifty percent on the circuit board. Designated the Bourns® Model MF-SD013/250-2, the device provides both tip and ring overcurrent protection and aids compliance with ITU-T K.20, K21 and K.45 industry standards as well as Telcordia GR-1089 intra building. Bourns® Multifuse® devices are an optimal solution for telecommunication applications including customer premise equipment and line cards.

"In response to growing demands for smaller devices that use less circuit board real estate, Bourns has innovatively packaged two Multifuse® PPTC devices together that protect both tip and ring lines into just one component instead of two,” said Paul Wiener, telecom market director for Bourns’ circuit protection products. “Bourns’ new Multifuse® products deliver superior overcurrent and overvoltage circuit protection and also comply with key industry standards.”

Pricing and Availability
Bourns® Multifuse® Model MF-SD013/250-2 is available now. For complete specifications, go to Bourns’ site at /ProductLine.aspx?name=polymer_ptc_resettable_fuses_multifuse. As a pricing reference, the new Multifuse® device with twin polymer PTC resettable fuses is priced from $0.50 in 400 piece quantities per reel.

Bourns®, the Bourns logo and Multifuse® are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

About Bourns

Bourns, Inc. is a leading manufacturer and supplier of automotive sensors, circuit protection solutions, magnetic products, microelectronic modules, precision potentiometers, panel controls and encoders and resistive products. Headquartered in Riverside, CA, Bourns serves a broad range of markets, including telecommunications, computer, industrial, instrumentation, automotive, consumer, non-critical life support medical, audio and various other market segments. Bourns products are manufactured according to ISO-9000 standards under Six Sigma quality programs. Additional company and product information is available at the company’s website at www.bourns.com.

Bourns® and the Bourns logo are trademarks or registered trademarks of Bourns, Inc. and may be used publicly only with the permission of Bourns and require proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Agency Contact:
Annette Keller
Keller Communication
(949) 640-4811
annettekeller@sbcglobal.net
  Company Contact:
Mikelyn Bridges
Bourns, Inc.
(951) 781-5397
mike.bridges@bourns.com