Search
Languages

Bourns Adds 12 New High Current Model Series to its Shielded Power Inductor Line

Manufactured with advanced powder cores, the new series provides high saturation/high heating current, low buzz noise and low magnetic field radiation

RIVERSIDE, Calif., August 9, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the addition of 12 new high current model series to its shielded power inductor line. The Bourns® Model SRP1038CC, SRP1245CC, SRP1265CC, SRP1770CC, SRP2313CC, SRP3012CC, SRP3020CC, SRP4012CC, SRP4020CC, SRP5020CC, SRP5030CC, and SRP7028CC Series power inductors are manufactured to provide engineers with distinct design advantages through either a carbonyl powder core or a metal alloy powder core, shielded construction to provide high saturation and high heating current, low buzz noise and low magnetic field radiation.

The 12 shielded power inductor series are designed to meet the high current density and increased inductor reliability requirements now present in a growing number of power electronics designs. This increased reliability, along with the series' extended operating temperature range of -40 to +125 °C and multiple footprints, make these inductors ideal power choke solutions for DC-DC converters and power supplies in consumer, industrial and telecom applications.

All 12 of the new high current shielded power inductor series are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf