Search
Languages

Bourns Introduces Air Coil Inductor Series with High Q, High Self-Resonant Frequency and Low Inductance Values

Offering lower losses and optimized for high frequency functionality, these new inductors give RF application designers a wider range of high Q solutions

RIVERSIDE, Calif., November 9, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced an air coil inductor series that features high Q, high self-resonant frequency and tight inductance tolerance. The Bourns® Model AC4842R Air Coil Inductor Series offers a high frequency, low loss solution that gives RF application designers a wider range of high Q solution options. Delivering a high Q value of at least 100 with inductance from 22 to 150 nanohenry (nH), these new air coil inductors are well-suited for today's high-frequency TV and radio receivers, radio transmitters and RF amplifier and tuning applications.

The series' features a wire coil design without a magnetic core, which provides significantly lower inductance values and offers superior functionality at high frequencies. Bourns designed the Model AC4842R Series with tight tolerance providing DC resistance from 4 to 33 milliohms, with 1.2 to 3.50 A maximum rated current and offering an operating temperature range from –25 to +125 °C. The Model AC4842R Series is also manufactured with an epoxy cover for added mechanical stability, and the series' surface mount design makes these air coil inductors ideal for pick and place processes.

The Bourns® Model AC4842R Series is available now, and is RoHS compliant*. For more detailed product information, please see: www.bourns.com/products/magnetic-products/air-coil-inductors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf