Search
Languages

Bourns Announces DIN-Rail Pluggable Surge Protective Devices Designed for High-risk Electrical Service Entrance and Branch Panels

Designed with an advanced hybrid MOV + GDT architecture, this new series delivers enhanced reliability and safety protection due to no leakage or follow-on current

RIVERSIDE, Calif., November 28, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its new Model 1260 Series Surge Protective Devices (SPDs). These AC hybrid SPDs are designed with an advanced MG (MOV + GDT technology) architecture that delivers enhanced reliability and safety protection due to the architecture's no leakage or follow-on current features. Bourns developed its latest series of hybrid SPDs as an optimum protection solution for electrical service entrances, branch panels, heavy industrial systems, EV charging stations or virtually any power circuit in installations without Lightning Protection Systems (LPS)/lightning rods.

The 1260 Series DIN-Rail pluggable design significantly streamlines installation and replacement, while the high short-circuit current rating of up to 50 kArms and impulse current capacity of up to 25 kA (10/350 μs) helps ensure that equipment is protected up to 100 kA (8/20 µs) per mode. In addition, this new series is compliant with IEC/EN 61643-11 Class I + Class II/T1+T2 standards, providing comprehensive protection for valuable equipment. To help designers satisfy a wide range of surge protection needs while enhancing reliability, Bourns® Model 1260 SPDs are available in multiple volt-ages and mode configurations.

Bourns® Model 1260 Series AC hybrid SPDs are available now and are RoHS* compliant. For detailed product information, please visit: www.bourns.com/products/surge-protective-devices/ac-surge-protective-devices.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf