Search
Languages

Bourns® DIN-Rail Data and Signal Surge Protective Devices Provide Two-Stage Protection for 1-Pair or 2-Pair Data Lines

Offering a highly-efficient overvoltage barrier solution, Bourns® Model 2510 and 2520 Series SPDs deliver both coarse (1st stage) and fine (2nd stage) protection

RIVERSIDE, Calif., November 29, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its Model 2510 and 2520 Series Data and Signal Surge Protective Devices (SPDs). The new DIN-Rail pluggable surge protectors offer a comprehensive solution to safeguard 1-pair and 2-pair data lines from damaging voltage surges and spikes. These robust protectors feature a two-stage protection scheme that utilizes Gas Discharge Tubes (GDTs) and fast bidirectional Silicon Avalanche Diodes (SADs) to provide both coarse and fine protection. This coordinated solution approach is ideal for a broad range of sensitive applications, including RS-232, RS-422 and RS-485 interfaces, low-voltage alarm circuits, high-frequency transmission systems, analog/digital communications and telecommunication equipment.

Bourns' new data and signal SPDs comply with UL 497B and IEC 61643-21, category D1/C1/C2/C3 standards. The Model 2510 and 2520 Series provide a maximum discharge current rating of 20 kA (8/20 µs) and are available in a range of service voltages to suit diverse applications, offering the flexibility to protect valuable equipment. Their pluggable design simplifies installation and maintenance, thereby helping to minimize downtime and maximize equipment productivity. Bourns® Model 2510 and 2520 Series data and signal SPDs are available now and are RoHS* compliant. For detailed product information, please visit: www.bourns.com/resources/rohs/surge-protective-devices/signal-and-data-line-surge-protective-devices.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf