Search
Languages

Bourns Expands its Model MF-ASML/X Series Multifuse® Overcurrent/Overtemperature Fuse Line with Higher 0.75 A Power Rated Model

New Polymer PTC Resettable Fuses Offer Higher Hold Current Options in an Ultra-compact 0402 Footprint

RIVERSIDE, Calif., December 11, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced it is expanding its Multifuse® Polymer PTC (PPTC) Resettable Fuse Model MF-ASML/X Series with a new higher power rated model. The Bourns® Model MF-ASML075/6 features a maximum 0.75 A (Ihold) rating and is designed to give developers of space-constrained applications greater overcurrent/overtemperature protection selection options in an ultra-compact 0402 footprint. In addition to the higher hold current and smaller footprint, the new model incorporates several key improvements, including increased voltage ratings (Vmax) and enhanced resistance stability. These enhancements are specifically crafted to cater to a wide array of applications, primarily as optimized protection solutions for low voltage DC ports commonly found in consumer products such as wearables, toys and gaming applications.

As the latest addition to the Multifuse® PPTC Resettable Fuse line, the Model MF-ASML075/6 is also based on Bourns' innovative freeXpansion™ technology. Developed more than 14 years ago, freeXpansion™ technology increases the performance of the fuse with the ability to handle higher currents and voltages, improves its resistance stability and allows for a smaller footprint. To help increase the reliability and longevity of all Multifuse® PPTC Resettable Fuses, including the MF-ASML/X model family, Electroless Nickel Immersion Gold (ENIG) plating is employed for their SMD terminals. ENIG plating uses a thin, uniform layer of gold over a layer of nickel that has been proven to offer outstanding corrosion resistance and excellent electrical conductivity. In contrast, traditional nickel-tin (Ni/Sn) plating can be susceptible to issues such as whisker formation, oxidation, and corrosion, which can lead to short circuits, subpar soldering and deterioration in electronic circuits.

The MF-ASML/X model family also adopts the unique Titanium carbide (WC) material, which features a lower resistance and is oxidation resistant in humid environments. A lower resistance is valuable because it contributes to higher power efficiency, while oxidation resistance aids in achieving an enhanced quality and reliability level.

The new addition to the Bourns® Multifuse® Model MF-ASML/X Series is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/docs/product-datasheets/mf-asml-x.pdf.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf