Search
Languages

Bourns Adds Multifuse® PPTC Resettable Fuse Series Developed for High Operating Temperature/High Operating Current Applications

New high power rated Model MF-RHS Series features low power dissipation in a small package designed to help to increase efficiency in motor and industrial designs

RIVERSIDE, Calif., January 2, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced its Multifuse® Model MF-RHS High Temperature Radial Leaded Polymer Positive Temperature Coefficient (PPTC) Resettable Fuse Series. Bourns' new fuse series answers the need for broader high temperature PPTC protection solutions that meet increased working temperature and high power rating requirements for a wide range of equipment, particularly in motor and industrial applications.

The new Model MF-RHS Series is based on Bourns' advanced design that increases resettable fuse performance and supports an operating temperature range up to 125 °C. Performance enhancements are comprised of an elevated 100 A maximum current rating (Imax), including a hold current rating range (Ihold) from 3.5 A to 13.0 A at 16 V maximum rated voltage and enhanced resistance stability in a smaller PPTC chip size. The series' smaller package dimension and low power dissipation can also help increase overall power application efficiency.

The Bourns® Multifuse® Model MF-RHS Series is available now and is RoHS compliant* and halogen free**. The series is also UL and CSA recognized and the products are manufactured in one of Bourns' IATF 16949 certified facilities. For more detailed product information, please see: www.bourns.com/products/circuit-protection/resettable-fuses-multifuse-pptc#rlths.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf