Search
Languages

Bourns Engineers Industry's First Planar Signal BMS Transformer

AEC-Q200 compliant signal transformer design includes basic electric insulation providing increased reliability/safety for high voltage EV and energy storage systems

RIVERSIDE, Calif., January 9, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released the industry's first planar signal BMS transformer. Meeting the need for planar technology that can provide reliable and safe communication in a growing group of high voltage electric vehicle (EV) and other high energy storage systems, the U.S. patented Bourns® Model SM91806 Planar Signal BMS Transformer meets basic electric insulation requirements per IEC 60664-1, IEC 61558-1 and IEC 62368-1 standards.

Planar-style signal transformers have been introduced to increase design flexibility and robustness. They are also known to deliver cost efficiency and reliability advantages over conventional wire wound transformer designs due to their multilayer PCB isolation and full automation. Offering these benefits and more, Bourns' new planar signal BMS transformer features a working voltage up to 1000 VDC, superior clearance/creepage distance features and complies with Overvoltage Category II. It also provides a partial discharge level up to 1200 V for ESS usage.

The Bourns® Model SM91806 Planar Signal BMS Transformer is available now and is RoHS compliant*. For more detailed product information, please see: www.bourns.com/products/magnetic-products/transformers-planar.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf