Search
Languages

Bourns Expands its SinglFuse™ SMD Fuse Line with Two High Voltage/Current Model Series

New Bourns® SinglFuse™ protectors now available in 0603 and 1206 packages deliver highly effective overcurrent protection in standard SMD sizes

RIVERSIDE, Calif., February 15, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the expansion of the Company's SinglFuse™ SMD fuse line. In power-based applications, efficiency plays a pivotal role, especially as end-products are increasingly sophisticated and have higher power consumption. The requirement for supporting components that feature a higher power rating in a compact form factor has become imperative. Bourns® Model SF-0603SP-R and Model SF-1206S-R Series meet these ongoing needs.

With the introduction of these two new SinglFuse™ SMD Fuse model families, designers of higher operating voltage applications can now select a more compact overcurrent protector. For example, the Model SF-0603SP-R Series is ideal for applications that operate at 48 VDC, and the Model SF-1206S-R Series is suitable for 12 VDC or 24 VDC operating systems where the operating current is over 10 A.

Bourns® SinglFuse™ SMD Fuses provide effective overcurrent protection in standard SMD sizes ranging from 0402 to 3812. Using Bourns' advanced design techniques, the new model series feature various voltage and current ratings, a wide operating temperature range and high-performance fuse characteristics.

The newly released model families utilize advanced Metal Foil technology, which is capable of handling higher currents in a compact form factor. This technology can support operating temperatures up to 125 °C, which is sufficient for most consumer, industrial and telecom applications.

The Bourns® Model SF-0603SP-R and SF-1206S-R Series SinglFuse™ SMD Fuses are available now. These models are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/circuit-protection/singlfuse-smd-fuses.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf