Search
Languages

Bourns Introduces BMS Signal Transformer Optimized for Higher Energy Storage Battery Management System Applications

Bourns® Model SM91801AL is developed for use with Analog Device Model LTC6815 Series, NXP Model MC33771C Series and Texas Instruments Model BQ79616

RIVERSIDE, Calif., February 28, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced a new single channel basic insulation transformer with a planar structure optimized for Battery Management System (BMS) applications. Bourns® Model SM91801AL is the next ‘first to market’ BMS signal planar transformer product Bourns has engineered, and is developed for use with several prominent semiconductor supplier IC series: Analog Device Model LTC6815 Series, NXP Model MC33771C Series and Texas Instruments Model BQ79616 ICs that are primarily used in multi-cell battery monitoring designs.

The latest BMS planar signal transformer from Bourns is AEC-Q200 compliant and automotive grade. It features a basic insulation layer that complies with IEC 60664-1 and IEC 62368-1 standards, and is manufactured using a fully automated process to deliver a high quality and cost-effective solution for next-generation applications. This BMS transformer offers a working voltage of up to 1000 VDC and a Hi-Pot isolation voltage up to 4300 VDC or 2500 VAC with an extended operating temperature range of -40 to +125 °C.

Bourns® Model SM91801AL is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/transformers-bms-aecq200.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf