Search
Languages

Bourns Introduces Family of Polymeric Thermal Cutoff (P-TCO) Devices to Protect USB-C Cables from Thermal Runaway Conditions

RIVERSIDE, Calif., February 27, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its new family of Polymeric Thermal Cutoff (P-TCO) devices designed to protect USB-C cables from destructive and potentially dangerous thermal runaway events. The new P-TCO family from Bourns offers an optimized overtemperature protection solution for USB C-C, C-B, and C-A connector configurations accommodating USB 3.2, 3.1, 3.0, and 2.0 protocols, as well as other types of data/charging cables.

Capable of delivering up to 100W of power, the USB Type-C connector features 24 pins in a smaller form factor than previous USB connector designs. While there are clear benefits to its enhanced power features and capabilities, there is also a downside. The combination of increased power and extremely tight pin spacing heightens the potential risk of safety hazards from thermal runaway conditions that could be triggered by dirt or liquid entering the connector and causing a short. Bourns' new P-TCO model series offers a combination of compact, ultra-low resistance thermal protection to help safeguard against these potentially dangerous overtemperature events.

The Bourns P-TCO family features surface mount packaging for automated assembly and low profiles for over-molding considerations. Designed to meet small footprint specifications, the new P-TCO family includes two series: P-TCO-U series in a 1210 footprint, and the P-TCO-N series in an ultra-compact 1206 footprint. Bourns offers the P-TCO device family with a 12V maximum operating voltage rating, and a 50A maximum operating current rating. Each series is available in three different models designed to provide protection for a variety of temperature-current combinations. The ultra-low resistance materials used in the P-TCO family enables both the P-TCO-U and P-TCO-N series to achieve initial resistance values as low as 2 mOhms and post-trip resistance values as low as 14 mOhms, thereby allowing the devices to achieve current-carrying capabilities as high as 4.5 A.

Bourns P-TCO-U and P-TCO-N series of USB-C protection devices as well as the company's entire line of overtemperature protection solutions will be highlighted at Battery Japan, February 27 to March 1, 2019 in booth # W4-68.

Bourns P-TCO family of devices is available now, are RoHS compliant* and halogen free**, are UL and TUV recognized for safety requirements, and are produced in Bourns' IATF-16949 approved facility in Xiamen, China. For more detailed product information, please go to: www.bourns.com/products/circuit-protection/polymeric-thermal-cutoff-devices-(p-tco).

* RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be “halogen free” if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.