Search
Languages

Bourns Extends Rotary Encoder Line with New Model Featuring High Detent Force with Smooth Tactile Feedback

Model PEC11H is Designed for Applications that Require a Rugged Menu-Select Encoder

RIVERSIDE, Calif., June 25, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of Model PEC11H as an extension to the company's rotary encoder product line. Bourns engineered its Model PEC11H encoder with an innovative ball/spring design that provides a strong, positive detent feel. This high force detent feature satisfies increasing end-user demands for more noticeable and smooth tactile feedback in a broad range of applications that require a rugged menu-select encoder such as in Professional Audio and Lighting, low/medium risk medical**, test/measurement and lab equipment, industrial automation controls and consumer white goods.

Bourns' new rotary encoder also features quadrature output with a 100,000 rotational cycle rating and a –25 °C to +70 °C operating temperature range. Delivering design flexibility, the Model PEC11H is offered in various resolutions and knurled and flatted shaft lengths as well as with a momentary push switch option.

The Model PEC11H encoder is RoHS* compliant, has an IP 40 dust seal rating, and is available now. For more detailed product information, please refer to the Bourns website: www.bourns.com/products/encoders/contacting-encoders

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.