Search
Languages

Bourns Announces AEC-Q200 Compliant Current-Compensated Dual Choke Filter Inductor Series with High Current Capabilities

New Model DR334A Line Filters Provide Superior Suppression of Common and Differential Mode Interference in Signal and Power Line Applications

RIVERSIDE, Calif., September 22, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced the Model DR334A Line Filter Series. These current-compensated dual choke filter inductors feature higher current capability than typical standard signal line common mode chokes, as well as high stray inductance and differential mode noise rejection. These capabilities make the Model DR334A series ideal line filter solutions for consumer, industrial and other market power line applications, or in applications where power is transferred over signal lines.

The new Model DR334A series is available in a bifilar-wound configuration to reach higher common mode impedance, and a sector-wound configuration to reach higher differential mode impedance at high frequencies. Offered in a compact, low profile (height 3.6 mm) size and in a broad range of inductance ratings from 11 µH up to 4700 µH, Model DR334A line filters allow designers to set the filter curve best suited to their application.

The Model DR334A series is AEC-Q200 compliant with an extended operating temperature range of –40 to +135 °C and has a rated voltage up to 80 VDC. In addition, the closed and ferrite toroid core construction of Bourns' latest line filter series delivers a more efficient and robust mechanical design.

The Bourns® Model DR334A Line Filter Series is available now, is RoHS* compliant and halogen free**. More detailed product information can be found at: www.bourns.com/products/magnetic-products/common-mode-chokes-aec-q200-compliant/

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.