Search
Languages

Bourns Releases Industry's First Power Transient Voltage Suppressors in Compact DFN Package

Bourns® PTVS1 and PTVS2 family of surface mount devices meet growing protection need for high 1 kA and 2 kA surge current solution in smallest DFN package

RIVERSIDE, Calif., August 2, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the industry's first Power Transient Voltage Suppressor (PTVS) product families available in the compact DFN package (8 mm x 6 mm x 2.5 mm) The Bourns® PTVS1 and PTVS2 surface mount series provide effective ESD protection to meet the growing demand for high surge current solutions that can also help designers save valuable PCB board space.

Another industry first from Bourns is that its Model PTVS2-xxxC-H series is the first PTVS device to feature the surge handling capability of 2 kA (8/20 μs). Compact packaging and higher surge protection requirements are trends in a wide range of next-generation AC and DC line protection applications such as those with exposed PoE ports or those that need high-power DC bus protection including 5G small cell, Remote Radio Units (RRUs) and Baseband Units (BBUs) in wireless base stations.

"With the release of our two new PTVS surface mount package product series, we are giving designers a much smaller solution with the same level of protection compared to existing PTVS devices that typically are available only in bulky over-molded or through-hole packages," said Jennifer Joseph, Semiconductor Product Line Manager at Bourns. "By helping our customers achieve smaller and more compact layouts, by as much as a 50 percent size reduction, Bourns' latest PTVS series also can reduce costs. In addition, it can offer increased design flexibility where the board space saved could be used to add more application features."

The new Model PTVS1-xxxC-H high current PTVS diode series consists of eight available part numbers with a maximum standoff voltage between 22 V to 86 V. This bidirectional PTVS Series delivers very low clamping voltage under surge conditions and excellent performance over temperature. The model PTVS1 series also meets IEC 61000-4-2 Level 4 ESD protection and 1 kA (8/20 μs) per IEC 61000-4-5 lightning protection. Similarly, the Bourns® Model PTVS2-xxxC-H PTVS diode family is offered in eight available part numbers with a maximum standoff voltage between 22 V and 86 V. Offering market-leading 2 kA (8/20 μs) per IEC 61000-4-5 lightning protection, this model series also meets IEC 6100-4-2 Level 4 ESD protection.

The Bourns® Model PTVS1-xxxC-H and PTVS2-xxxC-H high current PTVS diode series are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/diodes/power-tvs-diodes

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.