Search
Languages

Bourns to Present Two Technical Sessions at PCIM Europe 2019

RIVERSIDE, Calif., May 1, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, will display its broad portfolio of power conversion components for power electronics applications at the PCIM 2019 Europe Conference. The company will highlight its extensive experience in delivering successful magnetics designs and complete fast-turn prototypes, as well as the cost efficient and higher reliability and quality advantages provided by Bourns’ automated production expertise.

On Tuesday, May 7, Bourns will present a technical session entitled, “High-flux Density Amorphous Materials for High-Frequency Power Applications” at 15:00. Bourns’ second technical session, “Design and Development of a 20KW Transformer for Automotive Applications” will take place on Thursday, May 9, at 11:40.

Booth highlights:

  • Bourns transformers matched with chipsets providing isolated power and data
  • Extensive line of power conversion and power protection components
    • AEC-Q200-compliant components from IATF certified factories
    • Power and gate drive transformers, power inductors, common mode chokes
  • Custom design capabilities that meet application-specific requirements
    • Higher working voltages for isolated communication in BMS applications
    • Design support focused on efficiency and size

Where: PCIM Europe, Nuremberg DE
When: May 7 – 9, 2019
Location: Bourns Booth #445, Hall 7

You are invited to meet with a Bourns power electronics specialist to learn more about the design and time-to-market benefits the company can provide. Please contact Annette Keller, 707-947-7232, annettekeller1984@gmail.com.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf