Search
Languages

Bourns Introduces Chip LAN 10/100 Base-T Transformer Module

Saving Board Space, Bourns® Model SM41126EL Combines Discrete Chip LAN Transformers and Common Mode Chokes onto a PCB with a Ferrous Metal Shield

RIVERSIDE, Calif., May 6, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced a new Chip LAN 10/100 Base-T Transformer Module to help Ethernet and LAN-based application developers save valuable board space and increase design flexibility while meeting dynamic data line requirements. This new transformer integrates two Model SM453229-381N7Y Chip LAN transformers and two Model SRF2012A-801Y common mode chip inductors assembled on a PCB with a ferrous metal shield. This new model gives customers a simplified assembly solution that is pin-to-pin compatible with the traditional potted case LAN transformer and provides superior coplanarity. Designers also have the flexibility to use just the transformer or the common mode choke individually, which affords additional PCB placement freedom.

Manufactured using a fully-automated, high capacity process, Bourns® Model SM41126EL provides a consistent, highly reliable and cost-effective solution. The automated coil winding process is especially important as it ensures tight tolerances essential to electrical stability. This stability results in improved performance across a broad range of frequencies compared to manual winding processes. The low profile, small form factor module features an expanded temperature range of -40 to +85 °C, and is fully compliant with IEEE 802.3 making it ideal for use in LAN interfaces in a variety of telecommunication and network devices.

The Model SM41126EL Chip LAN 10/100 Base-T Transformer Module is available now and is RoHS* compliant. Design tools are also available to help streamline development. For more detailed product information, please refer to the Bourns website: www.bourns.com/products/magnetic-products/transformers-signal

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf