Search
Languages

Bourns Further Expands its SinglFuse™ Line with Five New Automotive-Grade SMD Fuse Model Families

RIVERSIDE, Calif., February 10, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today further expanded the company's SinglFuse™ product line with new automotive grade SMD fuse families. The five new SF-1206SA-W, SF-2410FPA-W, SF-2410FA-W, SF-0603HIA-M and SF-1206HIA-M model families are fully compliant with Bourns' internal AEC-Q200 equivalent test procedures to ensure rugged performance in a broad variety of applications that operate in certain harsh environments.

The SF-1206SA-W, SF-2410FA-W, and SF-2410FPA-W SinglFuse™ model series feature slow blow, fast-acting, and fast-acting precision fusing speeds in small form factor EIA1206 and 2410 packages. Utilizing Bourns' innovative PCB wire core design, these new families deliver enhanced voltage and current handling capabilities, more precise hot spot control along the fuse element, improved arcing suppression and inrush current withstand capability, and superior structural integrity when blown compared to older ceramic tube designs.

The new SF-0603HIA-M and SF-1206HIA-M model families were developed using Bourns' advanced multilayer ceramic design that enables enhanced voltage and current handling capabilities. Offered in small 1206 and 0603 package sizes, these models feature high inrush current withstand capabilities and time-lag fusing speeds.

Bourns continues to broaden its portfolio of SinglFuse™ SMD fuses to address the growing need for effective overcurrent protection in an increasing range of applications. As all sorts of systems and electronic applications have become more integrated and sensitive, overcurrent threats have the potential to inflict damage, reduce a product's lifespan and affect the efficiency of a device. Circuit protection is also important for emerging and next-generation applications such as IoT and smart sensor-based designs. These connected applications are particularly vulnerable to overcurrent events that can cause reduced reliability and failure to one or more devices in the network.

Available now, Bourns® SF-1206SA-W, SF-2410FPA-W, SF-2410FA-W, SF-0603HIA-M and SF-1206HIA-M models are UL 248-14 listed, RoHS** compliant and halogen free***. For additional product information, please see: www.bourns.com/products/circuit-protection/singlfuse-smd-fuses

*Meets Bourns' internal AEC-Q200 equivalent test plan.

**RoHS Directive 2015/863, Mar 31, 2015 and Annex.

***Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com