Search
Languages

Bourns Releases PDB241-GTR Series Guitar Potentiometer Product Extension

New product extension significantly increases the rotational life to 100,000 cycles to meet higher durability demands from frequent users

RIVERSIDE, Calif., May 12, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that the Company has released a product extension of its popular PDB241-GTR Series guitar potentiometers. This extension significantly increases the rotational life to 100,000 cycles, supporting the high-use demands of dedicated performers. With this extension, Bourns is also making a standard option available that offers a rotational life of 15,000 cycles.

In addition to the PDB241-GTR Series 100,000-cycle rotational life, it features low torque of 10 to 45 g-cm, a -10°C to +70°C operating temperature range as well as metal knurled and metal plain shaft options. These capabilities help ensure that when the guitar potentiometer is used in an instrument, the player gets the advantage of using a smooth-working component that more easily allows them to achieve the sound/effect they are trying to create on their guitar. This guitar potentiometer product extension is specifically suited for electric and bass guitars with thick bodies, and is engineered to meet players’ enhanced quality, reliability and durability expectations.

The Bourns® PDB241-GTR Series product extension is available now and is RoHS* compliant. For more detailed product information, please see: bourns.com/products/potentiometers/commercial-panel-controls.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com