Search
Languages

Bourns Expands Semi-Shielded Power Inductor Portfolio with New Series Featuring Higher Maximum Inductance Values

New models offer lower magnetic field radiation, providing a cost-effective alternative to fully shielded ferrite-based inductors

RIVERSIDE, Calif., July 10, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the expansion of its semi-shielded power inductors. Bourns has added five new product series to the existing Bourns® SRN-BTA family. These new products offer higher maximum inductor values – with some models doubling previous limits – while delivering lower magnetic field radiation. This provides a cost-effective alternative to fully shielded ferrite-based inductors. The semi-shielded construction combines the advantages of both non-shielded and shielded inductor designs, offering a robust and reliable solution for demanding power applications.

The new additions to the SRN-BTA family enhance product reliability with bottom-soldered lead-wires, providing increased mechanical strength and stability. These models are well-suited for applications in automotive systems, DC-DC converters, and power supplies across consumer, industrial and telecom electronics – particularly in applications requiring higher power inductors. These advancements deliver multiple benefits, including improved magnetic performance and greater efficiency.

The Bourns® SRN2010/2510/3010/3015/4018BTA Series Power Inductors are available now through Bourns’ authorized distribution partners. These models are AEC-Q200 compliant and automotive grade, meeting the rigorous standards required for automotive applications. These products are manufactured within a Bourns' IATF 16949 certified facility. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com