Search
Languages

Bourns Unveils Current Transformer Line with New Model that Features High Turns Ratio with Permalloy T-Core Construction

Bourns® Model PCP300-T414250S Current Transformer provides high permeability and low energy losses delivering excellent high frequency current sensing for power systems

RIVERSIDE, Calif., June 2, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today unveiled the Company’s new current transformer line with its Model PCP300-T414250S Transformer. The new model is made with high-efficiency permalloy material that helps reduce heat loss and energy consumption. This technology also enables fast power conversion rates with elevated precision, making this transformer ideal for power quality analysis. In addition, its advanced features support a wide range of rated current measurements, including high-frequency current sensing in power meters and motor load monitoring.

The Model PCP300-T414250S Current Transformer has a maximum primary continuous current of 300 A, with a dielectric strength of up to 3.5 kV, which are required to help ensure the safety of both equipment and personnel. Additionally, the new transformer features a protective coil housing design suitable for applications that operate in challenging environments. Bourns designed this new current transformer line to allow customers to achieve faster, higher stability and safe electricity monitoring and management.

The Bourns® Model PCP300-T414250S current transformer is available now through Bourns’ authorized distribution partners, and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/current-transformers.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com