Search
Languages

Offering Reliable Supply with Reduced Lead Times, Bourns Enters IGBT Market with Market-leading Power Efficiency Portfolio

Bourns' advanced trench-gate field-stop technology IGBTs provide low conduction/switching loss designed by the innovation leader power designers have trusted for 75 years

RIVERSIDE, Calif., August 8, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today entered the insulated-gate bipolar transistor (IGBT) market with the Company's first high-efficiency 600 V/650 V discrete product line co-packaged with a fast recovery diode (FRD). Designed using advanced trench-gate field-stop technology that provides greater control of dynamic characteristics, the five new Bourns® Model BID Series discrete IGBTs deliver lower collector-emitter saturation voltage (VCE(sat)) and lower switching losses compared to previous generation non-punch-through IGBTs. In addition, this structure provides a positive temperature coefficient that helps increase device longevity and reduce power requirements in high voltage and high current designs.

Because Bourns' new IGBTs are available in thermally-efficient TO-252, TO-247 and TO-247N packages, these devices can provide a lower thermal resistance Rth(j-c), making them ideal solutions for switch-mode power supplies (SMPS), uninterruptible power sources (UPS), induction heating and power factor correction (PFC) applications. Offering four voltage/current model options in 600 V/5 A, 600 V/20 A, 600 V/30 A and 650 V/50 A, Bourns® BID Series discrete IGBTs have been tested and qualified according to JEDEC standards for power switching products.

Bourns® BID Series IGBTs are available now and are RoHS compliant* and halogen free**. For more detailed product series information, please see: www.bourns.com/products/igbt

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.