Search
Languages

Bourns Launches Automotive Grade Semi-shielded Power Inductor Series Featuring High Operating Temperatures Up to 150 °C

AEC-Q200 compliant inductor series is constructed with magnetic silicon-based coating technology for superior magnetic shielding and supports higher operating temperatures

RIVERSIDE, Calif., June 22, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new AEC-Q200 compliant, automotive grade semi-shielded power inductor series that features a high operating temperature range from -40 °C up to 150 °C. The Bourns® Model SRN8040HA Series is constructed using the company's advanced magnetic silicon-based coating technology that offers superior magnetic shielding while also enabling higher operating temperatures.

Bourns' new high temperature inductors are designed to release lower magnetic field radiation compared to non-shielded inductors, and are also a more cost-efficient alternative to fully shielded ferrite-based inductors. The Model SRN8040HA series supports high current capacity with saturation current Isat ranging from 1.3 – 15 A and provides a heating current Irms range of 1.0 – 10.0 A. The features and capabilities of these inductors make them especially well-suited for DC-DC converters and power supplies in automotive, consumer, industrial, and telecom electronics applications where greater inductor reliability is a frequent requirement.

The Bourns® Model SRN8040HA semi-shielded power inductor series is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded/product/SRN8040HA

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf