Search
Languages

Bourns Announces Incremental Encoder with Long Rotational Life and Broad Range of Detent Options for Greater Customer Configurability

Bourns® Model PEC11J encoders feature an IP 40 rating and 100,000 cycle rotational life with switch options that allow adaptation to application-specific needs and environments

RIVERSIDE, Calif., June 26, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, announced today it is releasing the PEC11J series encoder as a drop-in replacement for the discontinued ALPS Model EC11J Series. This modified configuration of the Bourns® PEC11S series should enable customers to continue to support existing applications with no changes to their mechanical or electrical layouts. Testing is recommended to ensure compatibility with each customer's specific application. Samples are available upon request for testing.

Bourns® Model PEC11J Series encoders feature an IP 40 rating, a 100,000 rotational cycle rating and a -10 °C to +70 °C operating temperature range in a rugged, compact surface mount design. The encoders also offer an optional momentary switch function with standard and high actuation force capabilities that allow ease of adaption to application-specific needs and different environments. These features and capabilities make this product well-suited for a very wide range of applications including professional audio equipment and lighting consoles, white goods, low to medium risk medical* and diagnostic equipment, test and measurement equipment and industrial automation controls.

The introduction of the Model PEC11J Series is one of many new enhanced products planned by Bourns that will integrate advanced features and offer high reliability operation to help designers meet next-generation application requirements.

Bourns® Model PEC11J incremental encoders are available now and are RoHS compliant*. For more detailed product information, please see: www.bourns.com/products/encoders/contacting-encoders/product/PEC11J

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf