Search
Languages

At electronica China 2023, Bourns to Host Technical Forums on Advanced Power, Protection and Sensing Solutions for BMS Applications

TAIPEI, Taiwan, June 30, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection and sensing solutions, will showcase and demonstrate the company’s cutting-edge battery management system (BMS) solutions at the upcoming electronica China 2023, July 11 - 13. As a leader in developing and manufacturing one of the industry’s broadest portfolios of standard and custom magnetics, circuit protection and sensing components, Bourns will host a series of technical forums that provide helpful information for BMS designs. The technical forums will be held daily in Bourns booth #A228 and are designed so that industry professionals can gather and exchange insights on the latest trends and challenges in the BMS sector. The schedule of each day’s sessions will be provided in Bourns’ booth:

  • The latest BMS transformers and planar transformers
    • New designs provide higher current capability, superior heat dissipation, low parasitic leakage and EMI advantages
  • Innovative circuit protection solutions
    • Hybrid protectors deliver significantly enhanced surge performance, operational life and device reliability
  • High accuracy current sense resistors
    • Helps ensure efficient circuit operation and increases the life and functionality of the battery
  • Application demonstrations
    • Buck/boost and air core inductors that speed evaluation of SiC-based designs
    • Solutions for VCM functionality in smartphones

You are invited to attend the technical forums and also meet with Bourns’ component experts to learn about the company’s breakthrough products and advanced solutions for BMS, ADAS, on-board chargers, DC-DC converters and more! Please contact Josephine Chen to arrange an appointment: Josephine.chen@bourns.com

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf