Search
Languages

Bourns Announces High Performance DC Surge Protective Device Series

New general duty SPDs with pluggable/replaceable modules are designed to meet high-risk electrical service entrance and branch panel protection requirements

RIVERSIDE, Calif., July 5, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced a high-performance DC Surge Protective Device (SPD) Series. The Bourns® Model 1420A Series SPDs are a new family of DIN Rail general duty SPDs with pluggable/replaceable modules offering surge rates up to 50 kA in different configurations. Bourns specifically designed its Model 1420A Series SPDs to meet high-risk electrical service entrance and branch panel protection requirements of high power, sensitive energy generation and distribution terminals such as EV fast chargers, battery energy storage systems (BESS) and photovoltaic energy generation systems.

Sustained abnormal overvoltage high-energy surges can cause SPDs and/or MOVs to go into a thermal runaway condition that many times leads to device overheating and create a fire hazard. For this reason, Bourns' latest SPD products feature an Advanced Thermal Disconnector (TD+) that has a self-extinguishing mechanism that helps increase device safety during catastrophic end-of-life events. These new SPDs come with an additional window fault indicator and remote auxiliary output signal, which provides the ability to monitor the status of the device.

The Bourns® Model 1420A SPD Series is available now and is RoHS* compliant. This series is a UL recognized Type 4, Type 2 Location SPD and complies with IEC 61643-31 standards. For more detailed product information, please see: www.bourns.com/products/surge-protective-devices/dc-power-surge-protective-devices

Bourns について

Bourns, Inc. は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf