Search
Languages

Bourns Announces High Heat Tolerant Thick Film Resistor Series in a Compact TO-227 Package

The PF2270 Series power film resistors provide superior power dissipation and thermal efficiency for motor drives, power conversion and battery energy storage systems

RIVERSIDE, Calif., July 1, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new thick film resistor series that delivers high heat tolerance in a compact TO-227 package. The Riedon™ PF2270 Series Power Film Resistors by Bourns® are engineered to provide superior power dissipation based on their thick film technology design and excellent pulse handling capabilities that offer up to 300 W of power dissipation with heatsink. The low-inductance design and high-power dissipation ratings make these power film resistors ideal solutions for industrial motor drives, power conversion, battery energy storage systems and other high-performance electronic designs.

In addition to the series’ advanced TO-227 packaging enabling operating temperatures up to +175 °C, it also offers a wide resistance value range from 100 milliohms (mΩ) to 100 kiloohms (KΩ), and resistance tolerance options of 1 percent and 5 percent. These features deliver excellent current limiting, precise current measurement and superior capacitor discharge capabilities that benefit applications where high power density support and increased reliability are needed.

The Riedon™ PF2270 Series Power Film Resistors by Bourns® are available now through Bourns’ authorized distribution partners, and are RoHS* compliant. For more detailed product information, please see: /bourns.com/products/resistors/high-power-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf